Output Status
In Instrument View, the output status is shown in the title bar of each output tab.
The output status may include the following:
| Output Status | Display in Instrument View | Description |
|---|---|---|
| OV | OVP | over-voltage protection tripped |
| OC | OCP | over-current protection tripped |
| OT | OT | over-temperature protection tripped |
| SF | SF | a sense lead fault has been detected |
| PF | PF | a power-fail condition occurred |
| CC | CC | the output is in constant current mode |
| CV | CV | the output is in constant voltage mode |
| EDP | EDP | the output is disabled by excessive output dynamics protection |
| INH | INH | an external inhibit signal is received |
| CSF | CSF | a current sharing fault occurred |
| WTG | WTG | the output is waiting for a trigger |
| ON | ON | the output is on |
| OFF | OFF | the output is off |
| OVNEG | OV– | negative voltage protection tripped |
| CPPOS | CP+ | a positive power limit |
| CPNEG | CP– | a negative power limit |
| PROT | PROT | a coupled output protect occurred |
| UNPROT | UPROT | a user-defined protection signal has disabled the output |
| CLPOS | CL+ | a positive current limit |
| CLNEG | CL– | a negative current limit |
| IPKPOS | IPK+ | the output is in positive peak current limit |
| IPKNEG | IPK– | the output is in negative peak current limit |
| VLPOS | VL+ | a positive voltage limit |
| VLNEG | VL– | a negative voltage limit |
| UNR | UNR | the output is unregulated |
| CAL | CAL | the output is computing new calibration constants |
| CSF | CSF | a current sharing fault has occurred |
| MSP | MSP | output is disabled by the primary/secondary protection |